What components can be added to a T-slot aluminum framing system?
80/20 T-slot aluminum framing systems support a wide variety of
components that expand their functionality, including linear bearings, roller wheel assemblies, adjustable feet, casters, profile mounts, guides, and specialty hardware. These components allow manufacturers and designers to build everything from mobile workstations and machine guards to automation equipment and material handling systems while maintaining the flexibility of a modular aluminum framing system.
What are linear bearings used on aluminum extrusions?
80/20
linear bearings provide smooth, controlled motion along compatible aluminum extrusion profiles. They are commonly used in sliding doors, adjustable workstations, machine guarding, automation equipment, positioning systems, and inspection fixtures. Because they travel directly along the profile, they eliminate the need for separate guide rails in many applications.
How do roller wheel assemblies improve a modular framing system?
80/20
roller wheel assemblies create smooth rolling movement on compatible T-slot aluminum profiles, making them ideal for sliding panels, equipment carriers, adjustable machine guards, and material handling applications. Their design reduces friction while providing consistent, reliable motion for industrial equipment.
Are these components compatible with every T-slot aluminum profile?
Compatibility depends on the
profile series and slot dimensions. Many 80/20 components are designed for specific 80/20 profile families, including 10 Series, 15 Series, 25 Series, and metric profiles. Always verify profile compatibility before selecting hardware to ensure proper fit and performance.
Why are adjustable feet used on aluminum extrusion frames?
80/20 adjustable
leveling feet help stabilize equipment on uneven floors while allowing precise height adjustments. They're commonly installed on machine frames, industrial workstations, laboratory equipment, assembly tables, and automation systems where maintaining level surfaces improves stability, alignment, and overall performance.
What industries commonly use modular aluminum framing accessories?
80/20 modular aluminum framing accessories are widely used throughout manufacturing, industrial automation,
robotics, aerospace, automotive, medical device manufacturing, electronics assembly, laboratories, warehousing, packaging, and material handling. Their versatility makes them suitable for both production equipment and custom engineering projects.
Can these components be used for linear motion applications?
Yes. 80/20 linear bearings, roller wheel assemblies, guides, and related hardware are specifically designed to create controlled linear movement within
T-slot aluminum framing systems. They are frequently incorporated into adjustable workstations, positioning systems, machine guarding, pick-and-place equipment, and custom automation solutions.
Do these components require welding or custom fabrication?
No. 80/20 components are designed to install using compatible T-slot fasteners and
mounting hardware, eliminating the need for welding in most applications. This modular approach allows equipment to be assembled, modified, repaired, or expanded quickly while reducing downtime and fabrication costs.
What advantages do modular accessories offer over welded systems?
Unlike welded structures,
80/20 modular aluminum framing components can be repositioned, replaced, or expanded as operational requirements evolve. This flexibility reduces redesign costs, minimizes downtime, extends equipment life, and allows existing structures to be reused instead of replaced when production changes.
Are these components durable enough for industrial environments?
Yes.
80/20 components are engineered for demanding industrial environments and are commonly used in manufacturing facilities, warehouses, laboratories, clean rooms, and automation systems. Their durable construction provides reliable performance while supporting equipment that can be reconfigured as processes evolve.
How much maintenance do linear bearings and roller assemblies require?
Most 80/20
motion components require very little routine maintenance. Periodic inspection, keeping rolling surfaces clean, verifying fastener tightness, and monitoring normal wear will help maximize service life. Following recommended load capacities and installation guidelines also contributes to long-term performance.
Can these components be used to automate manufacturing equipment?
Absolutely. Motion components, profile mounts, and 80/20 specialty hardware are frequently integrated into automated manufacturing systems, robotic cells,
machine guarding, and conveyor equipment. Their modular design enables engineers to build systems that can be expanded, reconfigured, or upgraded without extensive redesigning.
Why choose 80/20 components for a modular aluminum framing system?
80/20 components are engineered to work seamlessly with the company's T-slot aluminum
extrusion profiles, providing reliable fit, consistent performance, and exceptional design flexibility. Whether you're building machine frames, automation systems, industrial workstations, or custom equipment, the modular approach makes assembly faster, simplifies future modifications, and helps reduce the total cost of ownership compared to traditional welded construction.