And the Winner is...
Congrats Michael!
Congratulations to Michael – you won the third photo contest of 2018. Michael will receive a $200 coupon to 8020.net for his model ocean! Michael explains this is "very accurate, controlled by state-of-the-art automation computers & human-machine interface. The system can duplicate any ocean wave phenomenon in model scale." How cool is that?!
Thanks for sharing and have fun shopping!
Want to Show Us Your Project?
Enter the Next Photo Contest Below
Browse through the gallery to view all contest pictures.
Past Winners

Forrest
Highway Mapper
Forrest built a highway mapper using both black and clear anodized profiles, along with 45-degree supports and a linear break kit.

Zack
Instrumented Treadmill
Zack built the treadmill to complete his master’s thesis; it examines the effects of military load carriage on vertical ground reaction parameters.

Lawrence
Solar Generator
Lawrence built a solar generator that houses a 1,400 kilowatt battery pack with an energy monitor and will be used by students to power devices like projectors and audio systems.

Laci
3D Printer
Laci designed and built a 3D printer! This is a high speed,
high volume printer that is fully functional and built with an 80/20 frame.

Kevin
Electric Car
Kevin sent in a picture of his street-legal electric car. This 30-horsepower vehicle can go up to 70 miles per hour and is built with an 80/20 frame.

James
Video Camera Jig
James sent pictures of his video camera jig and notes that using 80/20 products allows him to create an uncomplicated jig to mount a video camera on a teleprompter or tripod at a 90-degree angle. “It’s adjustable to any size camera and cost significantly less than a commercially available system.”

Jerry
Custom CNC Router
Jerry sent in a picture of his custom CNC router he is building completely from scratch. Jerry used a combination of 40 and 15 series profiles and notes that he "really liked that the joints went together very clean and are really tight."