Home Contact Us Careers Product Catalog Distributor Login






Made With 80/20 Stuff
Case Studies
Guarding & Enclosures
Workstations
Material Handling
Automation
Office & Displays
Furniture
Linear Motion
Robotic Fixtures
Out of The Box







Mailing List
E-Mail Address:

Full Name:

Format
HTML TEXT
80/20 Case Study - Radial Dolly
This Radial Dolly built by a video production D.I.Y. Guru was created with 15 Series smooth profiles and locking pivots to add a sweeping radius motion to camera shots.

Radial Dolly Photo #1

80/20 Case Studies

Radial Dolly Photo #2

80/20 Case Studies

Radial Dolly Photo #3

80/20 Case Studies

Radial Dolly Photo #4

80/20 Case Studies

Radial Dolly Photo #5

80/20 Case Studies

Radial Dolly Photo #6

80/20 Case Studies

Radial Dolly Photo #7

80/20 Case Studies

Radial Dolly Photo #8

80/20 Case Studies

Lasers were mounted on the wheel assemblies using custom machined brackets allowing the user to easily identify the angle of the wheels in relation to the subject so that the dolly will rotate around the calibrated point. The wheels eliminate the need for expensive track and the entire unit can be collapsed for easy travel to various locations.
Click Here - to see more 80/20 case studies.



Want to share your solution with the 80/20 world? Send us your 80/20 solution pictures and story to mypictures@8020inc.com

©2005 80/20 Inc. All Rights Reserved  See Our Terms and Conditions